Issue: Fls_MainFunction execute is too long runtime

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue: Fls_MainFunction execute is too long runtime

1,204 Views
DennyZhang
Contributor III

hi, nxp developer!

  I use the fee&fls to emualate the eeprom.  i config 16Byte block in fee.

  when i execute Fee_Write to write 18 blocks, and then call Fls_MainFunction  and Fee_Mainfunction. 

  Each block write, call Fls_MainFunction execution, close to 1ms.  18 loops, execute too long.
 
Ags_1-1726822520608.png
 
  Question 1: i use the RTD1.0.0, is the version of the flash erasing time? if RTD version cause,  how can i optimizing the problem in RTD1.0.0?
  Question 2: Could a misconfiguration of fee or fls have caused this problem? I've enabled the cache. What other configurations can be used to reduce execution time?
 
thank&regard
Ags
 
 
 
 
0 Kudos
Reply
1 Reply

1,161 Views
DennyZhang
Contributor III

debug the FLS_Mainfunction, i find the time-consuming function.

Ags_0-1727057958930.png

 

0 Kudos
Reply