Invalid Project Path: Include Path not (S32DS 2.2V)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Invalid Project Path: Include Path not (S32DS 2.2V)

跳至解决方案
13,693 次查看
Learner
Contributor III

Getting Error of invalid project path:

Steps performed:

  1. Uninstall and reinstall Design Studio
  2. Used New workspace
  3. Created a project with example project
  4. Compiled the project.

Please refer the snapshots (pasted+ attached)of Design Studio settings;

Learner_0-1623932892780.pngLearner_0-1623932892780.pngLearner_1-1623932945874.pngLearner_1-1623932945874.pngLearner_2-1623932970788.pngLearner_2-1623932970788.png

 

标记 (2)
0 项奖励
回复
1 解答
13,682 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check the Build Variables:

Build Variables.jpgBuild Variables.jpg
When delete the S32_SDK_PATH, I will get the same issue.
The value of S32_SDK_PATH exists by default after importing the project. 

${eclipse_home}../S32DS/software/S32SDK_S32K1xx_RTM_3.0.0

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
10,374 次查看
WenWenDar
Contributor II

I tried this method, it does not work too.

0 项奖励
回复
13,683 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check the Build Variables:

Build Variables.jpgBuild Variables.jpg
When delete the S32_SDK_PATH, I will get the same issue.
The value of S32_SDK_PATH exists by default after importing the project. 

${eclipse_home}../S32DS/software/S32SDK_S32K1xx_RTM_3.0.0

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复
13,305 次查看
Someoneq
Contributor I

I tried the above method, but to no avail. Can you help me further?

标记 (1)
0 项奖励
回复