Interrupt Signal in S32K324

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interrupt Signal in S32K324

ソリューションへジャンプ
1,921件の閲覧回数
hemanths
Contributor III

Hi Team,

Which pin can be used for interrupt signals?

 

0 件の賞賛
返信
1 解決策
1,907件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @hemanths 

As you know SIUL2 supports one to 32 external interrupts allocated to pads by the chip.

You can find which pin can be configured for external interrupt at the S32K344_Input Muxing tab of the S32K344_S32K324_S32K314_IOMUX file attached to the RM, there are shown all the pines that can be used for each interrupt. 

VaneB_0-1687801909932.png

 

B.R.

VaneB

 

元の投稿で解決策を見る

1 返信
1,908件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @hemanths 

As you know SIUL2 supports one to 32 external interrupts allocated to pads by the chip.

You can find which pin can be configured for external interrupt at the S32K344_Input Muxing tab of the S32K344_S32K324_S32K314_IOMUX file attached to the RM, there are shown all the pines that can be used for each interrupt. 

VaneB_0-1687801909932.png

 

B.R.

VaneB