Internal error during Start GDB Semihosting Job on S32DS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Internal error during Start GDB Semihosting Job on S32DS

8,133 次查看
hoona75
Contributor I

Hello Nxp,

 

Our third-party have faced a problem as below snapshot. They are using the PEMicro multilink USB. 
We checked the S32DS configuration together. But, not found any mis-configuration. 
Could you help us solve this problem. We are welcome any suggestions.

hoona75_0-1695804235813.jpeg

Thank you.

0 项奖励
回复
10 回复数

4,370 次查看
Dharanidharan_S
Contributor II

I found a way to resolve the issue. By luck if someone is using an older version 
Please follow the steps :

  1. Fetch the Plugin folder com.pemicro.debug.gdbjtag.pne_5.1.7.202112141853  from C drive & place it under same path in NXP S32DS Installation folder in respective PC.
  2. Goto Help->Installation Details ,
  3. Uninstall the latest version PEmicro Plugin 5.8.7 or any, S32K3XX Dev Package & RTD package
  4. Restart S32DS
  5. Goto Help->S32DS Extensions & Updates , you will be able to see this com.pemicro.debug.gdbjtag.pne_5.1.7.202112141853 under the list.
  6. Reinstall PEmicro Plugin 5.1.7,S32K3XX Dev Package & RTD package
  7. Restart S32DS
    [Note : I tried uploading this plugin com.pemicro.debug.gdbjtag.pne_5.1.7.202112141853 but its failed due to Size restrictions]

 

0 项奖励
回复

4,405 次查看
Dharanidharan_S
Contributor II

Any Update on rollback to previous version of pemicro Jtag debug?

0 项奖励
回复

4,344 次查看
Dharanidharan_S
Contributor II

I found a way to resolve this issue.
By luck If someone is using an older version

  1. fetch the plugin folder com.pemicro.debug.gdbjtag.pne_5.1.7.202112141853 from C drive & place it under the same path in your PC.
  2. Goto Help -> Installation Details, Uninstall the new version pemicro jtag debug 5.8.7 or any from the list & related S32K3XX Dev Package as it contains this plugin.
  3. Restart S32DS & Go to Help-> S32 Extensions & updates you will be able to see the older version
  4. Install the Pemicro Plugin, S32K3XX Dev package  & RTD Package

    Note: I tried uploading the older version com.pemicro.debug.gdbjtag.pne_5.1.7.202112141853 here but its failed due to size constraints
0 项奖励
回复

4,401 次查看
Dharanidharan_S
Contributor II
0 项奖励
回复

6,397 次查看
CY9
Contributor III

After almost half year

The same issus still on 5.7.6.202312041432 com.pemicro.debug.gdbjtag.pne.feature.feature.group 

waste my time 

8,100 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

It seems that the following thread might be related to this request:

Unable to Debug project using PEMicro Debugger - NXP Community

Is this correct? If not, please let us know.

0 项奖励
回复

8,073 次查看
RickYeh777
Contributor III

I got the same problem and worked around.
Just uninstall the latest update of PEmicro as below.
RickYeh777_0-1696409453102.png

And reinstall the previous version of them.

RickYeh777_1-1696409780462.png

 

0 项奖励
回复

8,038 次查看
julienrochette
Contributor I

Hi, where can you find an old version of the plugin or how did you roll back? I can not debug anything since the update.

thank you

8,014 次查看
RickYeh777
Contributor III

Two places to uninstall.

1. Help->Installation Details

RickYeh777_0-1696552072257.png

2.Help->S32DS Extensions and Updates

RickYeh777_1-1696552154667.png

Help->Install New Software, to get the previous version, 5.2.0.20220321...

RickYeh777_2-1696552415020.png

But if "C:\NXP\S32DS.3.4\S32DS\tools\gdb-arm" is cleared, you maybe need to run the install program of S32DS again.

7,514 次查看
ctunder77
Contributor I

Hello, 

   I have the error described in this thread and have tried to revert the components to the version in the thread but I only have access to a more recent subset of the components. Is there a way to get access to the "older" version that may work? I am not sure if I have another problem in my configuration so I have included what I have seen other threads mention.

Below are the versions of the debugging support and device expansion plugin I can access from the software installer.

ctunder77_1-1700019526452.png

This is my version of S32 Design Studio below and my installation details.

ctunder77_2-1700020515143.png

 

ctunder77_0-1700019448487.png

Thanks in advance.

0 项奖励
回复