Interface SD card over LPSPI0 with nxp s32k322 IC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interface SD card over LPSPI0 with nxp s32k322 IC

1,017件の閲覧回数
pratik_a
Contributor III

Hi, 

I want to interface SD card over LPSPI0 of the NXP S32K322 chip. So far, I have managed to add the LPSPI0 module through the components section in the config tools. I want to know how to initialize SPI0 in normal mode and make all the default configurations. I'm completely new to NXP development. Any help is appreciated.

0 件の賞賛
返信
2 返答(返信)

993件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @pratik_a 

The Real-Time Drivers (RTD) are software for AUTOSAR and non-AUTOSAR applications. From the information provided, I understand that you are using MCAL (AUTOSAR ) for this we provide a User Manual and Integration Manual of the drivers. You can access them by clicking on the driver in Config Tools, as shown in the attached image. 

VaneB_0-1707511557927.png

Also, in the most recent RTD releases, we only provide driver examples for K344, K358, and K396. Examples of other derivatives can be created based on these existing examples.

HOWTO: S32 Design Studio - Create a New S32DS Project from Example

 

B.R.

VaneB

0 件の賞賛
返信

917件の閲覧回数
pratik_a
Contributor III

Hi @VaneB 

Thank you for the quick reply. It's been really helpful.

 

0 件の賞賛
返信