Installing DS version 3.4 issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing DS version 3.4 issue

1,383件の閲覧回数
cw20
Contributor II

Hi,

 

I'm having some issues after downloading DS version 3.4. This is everything I have installed:

cw20_0-1685547963289.png

 
 

image.png

 

The main issue is that the GCC cannot be found in the path so the project cannot build properly. I have gcc v10.2 installed, however, there is an orphaned configuration issue: 

image (2).png

Additionally, when I try to run the Adc example project, I can't open the peripheral view and the SDK is unavailable for the project, so there are no SDKs available:

image (4).png

image (3).png

0 件の賞賛
返信
1 返信

1,365件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Adc_example_S32K344 seems to come from S32K3 RTD 2.0.1, but only S32K3 RTD 2.0.0 is installed in S32DS Extensions and Updates. Please offline install SW32K3_RTD_4.4_2.0.1_DS_updatesite_D2207.zip by refer to Offline Package Installation Setup. Or import Adc_example_S32K344 from S32K3 RTD 2.0.0.

(S32K3 Standard Software -> Automotive SW - S32K3 - Real-Time Drivers for Cortex-M -> S32K3 Real-Time Drivers Version 2.0.1 -> SW32K3_RTD_4.4_2.0.1_DS_updatesite_D2207.zip)

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信