IPCF v3.7.0 problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPCF v3.7.0 problem

2,427件の閲覧回数
chuanlin
Contributor III

Can S32DSV3.5 import IPCF routines suitable for S32K324 from IPCF V3.7.0?

0 件の賞賛
返信
5 返答(返信)

2,419件の閲覧回数
chuanlin
Contributor III

Hello, I found a make method routine in IPCF v3.6.0. Is the routine integrated into S32DS currently not open.

0 件の賞賛
返信

2,416件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

if I understand your question correctly - you like to build IPCF example from command line by make command?

 

The procedure is described step by step in  SW32K3_IPCF_3.6.0_D2206_UserManual.pdf  - page 22.

 

 

 

 

0 件の賞賛
返信

2,403件の閲覧回数
chuanlin
Contributor III

Hello:

 No, I know the 'make' method, But ,there are no S32DS engineering examples related to S32K324 found here.

0 件の賞賛
返信

2,385件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I checked the content of IPCF package and based on README.rst file - the s32_rtd_S32K3XX example supports S32K324. At least in stand alone version (the .exe file installer for IPCF). 

0 件の賞賛
返信

2,420件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

no, as you can see in Release Notes - S32K3 IPCF v3.7.0 supports S32K358 device. 

 

Please use your existing threads - this is your fourth thread related to the same topic. 

0 件の賞賛
返信