IPCF problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPCF problem

1,046件の閲覧回数
chuanlin
Contributor III

chuanlin_0-1686045667496.png

 

Hello,If implementing IPCF Core0->Core1 and Core1->Core0 information exchange, does this configuration item need to add two Unmanaged Channels?

0 件の賞賛
返信
1 返信

1,003件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hello @chuanlin,

No, the channels on each core is independence, but need to be configure symmetrically. (If on core 1 you have (unmanaged, managed, managed) then core 0 also need the same channel with same order (unmanaged, managed, managed), pools number, pool size.)

Incase of using Unmanaged, each core will use it own unmanaged channel to communicate with the other core.

Best regards,

Dan

0 件の賞賛
返信