IPCF problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IPCF problem

1,094 Views
chuanlin
Contributor III

chuanlin_0-1686045667496.png

 

Hello,If implementing IPCF Core0->Core1 and Core1->Core0 information exchange, does this configuration item need to add two Unmanaged Channels?

0 Kudos
Reply
1 Reply

1,051 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hello @chuanlin,

No, the channels on each core is independence, but need to be configure symmetrically. (If on core 1 you have (unmanaged, managed, managed) then core 0 also need the same channel with same order (unmanaged, managed, managed), pools number, pool size.)

Incase of using Unmanaged, each core will use it own unmanaged channel to communicate with the other core.

Best regards,

Dan

0 Kudos
Reply