IPCF installation issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPCF installation issues

2,559件の閲覧回数
chuanlin
Contributor III

Step 1 : Downloaded NXP_Multi_Installer_17.05.23.095453_setup.exe installation is complete.

chuanlin_0-1684314379814.png

Step 2 : SW32K3_IPCF_3.4.0_D2112_updatesite.zip   Unable to install properly through Help ->Install New Software ->Add ->Archive.

chuanlin_1-1684314560101.png

Step 3: SW32K3_IPCF_3.4.0_D2112_ReleaseNotes.pdf Document cannot be opened

What is the reason for this?

 

 

 

0 件の賞賛
返信
1 返信

2,541件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

please use one thread. You have three treads related to the same stuff. 

 

So, the reason why you can't open release_notes pdf file is that the file is corrupted. Original SW32K3_IPCF_3.4.0_D2112_ReleaseNotes.pdf file has 265 800 bytes (in attachment). Your file has 49k.

 

As I said IPCF v3.4.0 is NOT compatible with S32DS v3.5:

jiri_kral_1-1684325531500.png

 

Please use older S32DS version or newer IPCF version. 

0 件の賞賛
返信