S32K118EVB doesn't work with PE Micro Multilink Universal FX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K118EVB doesn't work with PE Micro Multilink Universal FX

Jump to solution
697 Views
bjs
Contributor III

Hi,

I'm working with s32k118evb. I can use on board OpenSDA debugger to download image and debug but the board doesn't work with PE Micro Multilink Universal FX.

I also have a s32k144evb board and this board works well with the same PE Micro Multilink device. 

Can I use my PE Micro Multilink with this board?

Bruce

 

0 Kudos
Reply
1 Solution
663 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Bruce,

You can use PE Micro Multilink with this board.
From the photo it looks like J15 is not connected, but this jumper is used to power VDD_MCU. Please make sure the MCU is powered and try to debug it. 

J15 S32K118EVB2Q048.png
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
664 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Bruce,

You can use PE Micro Multilink with this board.
From the photo it looks like J15 is not connected, but this jumper is used to power VDD_MCU. Please make sure the MCU is powered and try to debug it. 

J15 S32K118EVB2Q048.png
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
656 Views
bjs
Contributor III

Thanks for the info. Now it works after J15 connected.

 

0 Kudos
Reply