IAR Compiler plugin for S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IAR Compiler plugin for S32DS

1,113件の閲覧回数
AdithyaJayaram1996
Contributor III

We are currently working on a project using S32K148 with S32 Design Studio 3.5 (S32DS 3.5) and RTD 2.0.0 along with FreeRTOS. As part of our development, we are considering switching to the IAR compiler and need guidance on its compatibility with S32DS.

Our Key Requirements:

  1. Which IAR compiler version is suitable for integration with S32DS 3.5?

  2. Is there an official IAR plugin available for S32DS 3.5, and how can we install it?

  3. Are there any known issues or limitations when using IAR with S32K148 + RTD 2.0.0 + FreeRTOS?

  4. Is there any migration guide or documentation for transitioning from the default GCC toolchain to IAR within S32DS?

Additionally, if IAR is not directly supported via a plugin, is there any alternative way to configure S32DS to build and debug using the IAR toolchain?

タグ(1)
0 件の賞賛
返信
1 返信

1,090件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can use for example IAR v9.32 - but any other version offered by IAR plugin manager can be used. Here is document how to install IAR plugin: 


https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Install-IAR-Eclipse-plug-in-into...

0 件の賞賛
返信