How to switch processor from S32K344 to S32K312

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to switch processor from S32K344 to S32K312

Jump to solution
1,096 Views
Eason_L
Contributor III

Hi,

According to S32DS 3.4 help contents in below picture, but I can't find the path "File > Switch processor". Is there anyway to change it?

Eason_L_0-1691112385157.png

 

 

Thanks,

Eason

Tags (2)
0 Kudos
Reply
1 Solution
1,074 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Eason,

You can Switch package for Processor in S32CT(S32 Configuration Tool) of S32DS. But unfortunately you cannot switch the processor from S32K344 to S32K312. It is recommended to create a new S32K312 project and refer to the S32CT of the original project.

Switch package for Processor S32DS S32K312.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,075 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Eason,

You can Switch package for Processor in S32CT(S32 Configuration Tool) of S32DS. But unfortunately you cannot switch the processor from S32K344 to S32K312. It is recommended to create a new S32K312 project and refer to the S32CT of the original project.

Switch package for Processor S32DS S32K312.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply