‌How to specify the destination and source addresses for SPI DMA in S32K366 within S32DS 3.6 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

‌How to specify the destination and source addresses for SPI DMA in S32K366 within S32DS 3.6 ?

245件の閲覧回数
zhangzhixing
Contributor III

‌How to specify the destination and source addresses for SPI DMA in S32K366 within S32DS 3.6 and RTD5.0?

タグ(1)
0 件の賞賛
返信
1 返信

216件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @zhangzhixing 

To better understand the SPI communication using DMA, an example project named "Spi_Transfer_S32K396" is provided with the RTD 5.0.0 package. This example demonstrates how to configure and use SPI with DMA through the MCAL drivers.

Additionally, you may find it helpful to refer to the following community thread, which includes examples for the S32K344 device. While this is a different MCU from the one you are using, the implementation is quite similar and could serve as a useful reference.

Example S32K344 SPI Transmit & Receive Using DMA DS3.5 RTD500

 

BR, VaneB

0 件の賞賛
返信