According to user manul said: ADC2 S8 is driven by GPIO_PAD133 (default) and GPIO_PAD45 (mux_mode). but how to and where to set the DCM register in EB Tresos studio? I can not find it in Platform Mcl Mcu and other likely modules?
Platform:RTD2.0,ASR4.4 EB Tresos 28
已解决! 转到解答。
 
					
				
		
 Robin_Shen
		
			Robin_Shen
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Sorry. As far as I know, this DCMRWF4 related bug was fixed in S32K3 RTD 3.0.0. It should be clear after checking the Siul2_Port_Ip_WriteDCMConfiguration.
Sorry for causing confusion, the RTD release note only excerpts the bug description of the internal system and does not include the detailed information of the bug. So ADC2_S8 also has problems.
Did you configure the pin in PortContainer?
 
					
				
		
 Robin_Shen
		
			Robin_Shen
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi
Please refer to the discussion in S32K344 ADC: HAS_ADC_INTERLEAVE problem
Sorry for the inconvenience we bring you!
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
 
					
				
		
 Robin_Shen
		
			Robin_Shen
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Sorry. As far as I know, this DCMRWF4 related bug was fixed in S32K3 RTD 3.0.0. It should be clear after checking the Siul2_Port_Ip_WriteDCMConfiguration.
Sorry for causing confusion, the RTD release note only excerpts the bug description of the internal system and does not include the detailed information of the bug. So ADC2_S8 also has problems.
Did you configure the pin in PortContainer?