How to program S32k144 with Multilink when use MBDT?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to program S32k144 with Multilink when use MBDT?

ソリューションへジャンプ
951件の閲覧回数
nujia
Contributor I

I use MBDT generate the code and program the S32k144 evb with OpenSDA interface.

but  i want to use Multilink to download the srec file. 

first step: generate the code wiht MBDT and compile the code.

second step: Run the S32DS, flash with elf file. 

How to automatic download the code without OpenSDA?

Thx.

0 件の賞賛
返信
1 解決策
941件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi nujia,

The MBDT is currently supported on the MBDT community only.
The community is monitored daily by our experts on MBDT.
Can you please post the question there?
https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/bd-p/mbdt
Thank you for your understanding!

You can refer to these two posts, but it is recommended to re-ask to get the latest answer:
Dears,how can i use multilink download code with Matlab Sumilink.
Flashing S32K144 with PEMicro Multilink from Toolbox

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
942件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi nujia,

The MBDT is currently supported on the MBDT community only.
The community is monitored daily by our experts on MBDT.
Can you please post the question there?
https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/bd-p/mbdt
Thank you for your understanding!

You can refer to these two posts, but it is recommended to re-ask to get the latest answer:
Dears,how can i use multilink download code with Matlab Sumilink.
Flashing S32K144 with PEMicro Multilink from Toolbox

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信