How to integrate TCP/IP stack for S32K3 with FreeRTOS in S32 Design Studio Project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to integrate TCP/IP stack for S32K3 with FreeRTOS in S32 Design Studio Project

706 次查看
jakub_mielczare
Contributor IV

Hello,

My team is working on a project with FreeRTOS and TCP/IP for S32K324 (or later S32K328).

Could you please advise how to integrate NXP TCPIP_STACK S32K3XX 2.0.0 with FreeRTOS FREERTOS S32K3_S32M27X 4.0.0 in a S32 Design Studio Project (Ubuntu)?

Thank you,

Jakub

0 项奖励
回复
3 回复数

688 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @jakub_mielczare 

Just to add a bit more information to what I shared in your other post (How to integrate FreeRTOS in a project for S32K3 in S32 Design Studio for Ubuntu? starting with RTD AUTOSAR R21-11 Version 4.0.0, support and testing for S32K3x8 devices (excluding the S32K388) was included.

 

BR, VaneB

0 项奖励
回复

634 次查看
jakub_mielczare
Contributor IV

Hi Vane,

So if I would use the RTD AUTOSAR R21-11 Version 4.0.0 and the mentioned FreeRTOS package, do I need TCP/IP stack mentioned earlier or TCP/IP stack is included in the RTD / FreeRTOS packages?

If not included, can you share an integration guide and which TCP/IP package specifcally should be used in this case?

Thank you,

Jakub

标记 (3)
0 项奖励
回复

620 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @jakub_mielczare 

The compatible TCP/IP stack version for this RTD is 1.0.4. You can download it from: S32K3 Reference Software → Automotive SW - S32K3 - Stacks → SW32K3_TCPIP_1.0.4_D2401.

0 项奖励
回复