Hi @jakub_mielczare
To make sure I can provide the most helpful support, I would like to point out a few things that might affect your implementation:
The S32K3 Real-Time Drivers (RTD) Version 2.0.1 were developed and tested using S32 Design Studio for S32 Platform version 3.4. Because of this, we cannot guarantee full compatibility or correct functionality with other IDE versions.
At the moment, there is no RTM version of the RTD officially compatible with this IDE version. However, in my personal experience, the S32K3_S32M27x Real-Time Drivers AUTOSAR R21-11 Version 5.0.0 has worked without issues in this environment.
Regarding, the FreeRTOS package, the SW32K3 FreeRTOS 10.6.0 Version 4.0.0 package depends on S32K3_S32M27x RTD AUTOSAR R21-11 Version 4.0.0, which means it is not compatible with the RTD version you are currently using.
Please note that all software package dependencies and required IDE versions are detailed in each package’s release notes, so it is always a good idea to double-check those for compatibility.
Lastly, please note that RTDs are not supported on Linux platforms only on Windows. Even if installation is successful, you may encounter issues due to Linux’s case-sensitive file system. This limitation has been discussed in the following thread:
Problems with Lpi2c_Ip_MasterConfig and Lpi2c_Ip_SlaveState struct generation on S32 DS for S32K344
BR, VaneB