How to correctly configure and use the "Mem Start Flash Access Notification" parameter for S32K312?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to correctly configure and use the "Mem Start Flash Access Notification" parameter for S32K312?

3,153件の閲覧回数
Chris-Sun
Contributor II

I am currently working on a project involving the S32K312 chip and using S32DS for configuring the Flash.
Errors occurred after configuring the "Mem Start Flash Access Notification" parameter for S32K312.
Could anyone please provide some guidance or advice on how to configure and use the "Mem Start Flash Access Notification" parameter correctly?

The version information:
 

S32DS: 3.5

RTD: S32K3_RTD_3_0_0_D2303_ASR_REL_4_7_REV_0000_20230331

1.png

Thank you in advance for your assistance.

 
0 件の賞賛
返信
11 返答(返信)

2,695件の閲覧回数
RogerFranca
Contributor II

Hi!

I have the same problem, but I already have a large part of my application developed and changing RTDs would not be ideal.

Would there be any explanation to solve the C40 problem with the RTD setup in the first image published in this topic?

0 件の賞賛
返信

2,675件の閲覧回数
Chris-Sun
Contributor II
Unfortunately, I was only able to solve this problem by upgrading the version of RTD and couldn't find any other solution.

3,139件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Chris-Sun

Could you please have a try to update the code.

Senlent_0-1709027909919.png

 

If the error still exists, I hope you can provide your project

0 件の賞賛
返信

3,127件の閲覧回数
Chris-Sun
Contributor II

Hi @Senlent 

Thank you for your response to my post.

I tried to update the code, but there are still errors.
2.png
 
Attached is the project I used.
 
Best regards,
Chris
0 件の賞賛
返信

3,108件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Chris-Sun

I imported the project you provided, and the interface displayed is a little different.

however I didn't find any problems.

Senlent_0-1709087649466.png

 

0 件の賞賛
返信

3,106件の閲覧回数
Chris-Sun
Contributor II

Hi @Senlent 

Thank you for your response to my post.

According to the screenshot you provided, the configuration pages for C40 are different, and the "Mem Start Flash Access Notification" configuration option is missing. (The error I encountered during configuration might be caused by this option.)
Is it possible that we are using different versions? 
 
The version information:
 

S32DS: 3.5

RTD: S32K3_RTD_3_0_0_D2303_ASR_REL_4_7_REV_0000_20230331

Best regards,
Chris

0 件の賞賛
返信

3,104件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Chris-Sun

Can you try installing this version
There are many versions of RTD 3.0.0, and I can't adapt to all of them on my computer at the same time.

Senlent_0-1709089082474.png

 

0 件の賞賛
返信

3,020件の閲覧回数
Chris-Sun
Contributor II
Hi @Senlent 
After using the RTD version you mentioned earlier, I no longer receive any errors, and the graphical interface of the configuration item has also changed.
Does this imply that only specific version RTD support the "Mem Start Flash Access Notification" configuration?
3.png
0 件の賞賛
返信

3,006件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Chris-Sun

I don’t think RTD has such obvious problems.
As I replied to you before, since the versions you and I use are different, I cannot help you troubleshoot the problem (unless I install an older version of RTD). I think this should still be a problem with certain configuration option settings.

0 件の賞賛
返信

3,016件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Chris-Sun

 I think "Mem Start Flash Access Notification" is just same with the below highlight part.

Senlent_0-1709540828848.png

 

0 件の賞賛
返信

3,010件の閲覧回数
Chris-Sun
Contributor II
Yes.
What I mean is, previously when I used the following RTD version and configured "Mem Start Flash Access Notification", it resulted in many errors (as shown in the image I added earlier).
4.png
Then I installed this version of RTD and configured "Mem Start Flash Access Notification", and there were no errors. Additionally, the graphical interface of the configuration has changed.
5.png
From this, can we conclude that the configuration of "Mem Start Flash Access Notification" has issues in a certain version of RTD and works properly in other versions?
 
Best regards,
Chris
0 件の賞賛
返信