How to Drive a Motor with Single Resistance Sampling

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to Drive a Motor with Single Resistance Sampling

2,137 次查看
zhouqicheng
Contributor I

Hello, do you have a motor drive routine for single resistance sampling? Or how to use the three-phase resistor program to change

0 项奖励
回复
3 回复数

2,123 次查看
RadekS
NXP Employee
NXP Employee

Hi zhouqicheng,

The S32K motor control kits could be found on the web page http://nxp.com/AutoMCDevkits or directly Arm-based kits at http://nxp.com/S32KDevKits

Currently, the Single-shunt example software contains SW packages for MCSPTE1AK116, MCSPTE1AK144 kits, and MCSXTE2BK142 evaluation board. Look for "1Sh" in the project folder name.

RadekS_0-1683901854688.pngRadekS_1-1683901854684.pngRadekS_2-1683901854689.png

 

Unfortunately, the Single-shunt example software for S32K3 is still in progress.

 

The same is valid for application notes for this version of the software example code - they are not publicly available yet. However, you may look at AN5327: 3-phase Sensorless Single-Shunt Current-Sensing PMSM Motor Control Kit with MagniV MC9S12ZVM. The current sensing and reconstruction technique is described in chapter 3.3.2 Phase currents reconstruction.
It is for different MCU, but the principle is the same.

I hope it helps you.

Bes regards

RadekS

0 项奖励
回复

2,067 次查看
zhouqicheng
Contributor I
hello ,the Single-shunt example software contains SW packages for MCSPTE1AK116, MCSPTE1AK144 kits, and MCSXTE2BK142 evaluation board. Is there a link? Or can you send it directly to me? mailbox 929592061@qq.com, Thank you
0 项奖励
回复

2,059 次查看
RadekS
NXP Employee
NXP Employee

Yes, sure. Here are the links:

MCSPTE1AK116 kit and direct link to the MCSPTE1AK116-SW

MCSPTE1AK144 kit and direct link to the MCSPTE1AK144-SW

MCSXTE2AK142 kit and direct link to the MCSXTE2AK142-SW

The nxp.com/AutoMcDevKits is an upper-level web page and above mentioned kits may be found under the Arm-based Development Solutions section.

Best regards

RadekS

0 项奖励
回复