How do I stop the LPIT counter from counting while jlink is debugging In S32K118

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I stop the LPIT counter from counting while jlink is debugging In S32K118

1,053 Views
Xiao-xiao-pang
Contributor I

While I was debugging the code, the LPIT timer count was decreasing while the code was running.

triggering the LPIT interrupt。I don't expect the counter value of LPIT0 to change when in debug。How to set the register?

4f08ae2d72aaab73ab09b733fffe9b2.png

0 Kudos
Reply
1 Reply

1,031 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Xiao-xiao-pang 

Could you help me confirmin if you are using the EVB? Also, which software and version are you using?

0 Kudos
Reply