How do I stop the LPIT counter from counting while jlink is debugging In S32K118

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I stop the LPIT counter from counting while jlink is debugging In S32K118

1,049件の閲覧回数
Xiao-xiao-pang
Contributor I

While I was debugging the code, the LPIT timer count was decreasing while the code was running.

triggering the LPIT interrupt。I don't expect the counter value of LPIT0 to change when in debug。How to set the register?

4f08ae2d72aaab73ab09b733fffe9b2.png

0 件の賞賛
返信
1 返信

1,027件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Xiao-xiao-pang 

Could you help me confirmin if you are using the EVB? Also, which software and version are you using?

0 件の賞賛
返信