HSE active passive block fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HSE active passive block fail

ソリューションへジャンプ
6,290件の閲覧回数
liangyouchao
Contributor I


CHIP:     S32K312

LC:    HSE_LC_CUST_DEL

HSE FW ver:    1.13.0.1.2.1

My code is 90KB, I copy 128KB data from address 0x00400000 to 0x00500000, and then execute the service HSE_SRV_ID_ACTIVATE_PASSIVE_BLOCK, but the hseSrvResponse code returns HSE_SRV_RSP_NOT_ALLOWED.

#define HSE_SRV_RSP_NOT_ALLOWED                 ((hseSrvResponse_t)0xAA55A21CUL)  /**< @brief The operation is not allowed because of some restrictions (in attributes, life-cycle dependent operations, key-management, etc.). */
 

what could be the reason for this?

 

0 件の賞賛
返信
1 解決策
6,191件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @liangyouchao 

please try to update the FW to latest version which is 0.2.6.0.

The correct file for AB Swap version (which ensures that OTA flag is enabled by HSE) is this one:

s32k3x2_hse_fw_1.13.0_2.6.0_pb221129.bin.pink

Update also the SBAF. It can be found in the 0.2.6.0 FW package too. It will ensure that all the HSE services will be available.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
6,253件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @liangyouchao 

Although the HSE RM does not specify the Super User (SU) right requirements for partition swap service, SU is needed.
LC CUST DEL has SU rights by default but user rights can be forced (from HSE RM):

"The execution rights after reset in LC states CUST_DEL and OEM_PROD can be forced to User rights configuring the “Start as User” option within hseAttrExtendCustSecurityPolicy_t and hseAttrExtendOemSecurityPolicy_t attributes."

Could you confirm you are not forcing user rights?


Also, it should be noted that the partition swap service ACTVATE Passive block can be given once in a reset cycle, so if you call the service twice it also returns error "HSE_SRV_RSP_NOT_ALLOWED".

Regards,

Lukas

0 件の賞賛
返信
6,216件の閲覧回数
liangyouchao
Contributor I

Hi Lukas, Thank you for your reply.

My project is a basic project, s32k312 HSE function has just started testing, I have not done any operations, such as advance LC, program ADPK key, and format HSE key catalogs, etc., so the chip status is default.

The test code and allowed results are shown in the following figure:

void hse_init()
{
    hseStatus_t        HseStatus;
    hseSrvResponse_t   HseSrvResponse;

    OsIf_Init(NULL_PTR);

    Crypto_Init(NULL_PTR);

    HostFlash_Init();

    /* read HSE FW Version */
    HseSrvResponse = HSE_GetVersion(&HseFwVersion);
    LOGI("HSE Version: %d.%d.%d.%d.%d.%d\r\n", HseFwVersion.reserved, HseFwVersion.socTypeId, HseFwVersion.fwTypeId, 
    HseFwVersion.majorVersion, HseFwVersion.minorVersion, HseFwVersion.patchVersion);

    /* read Lifecycle */
    HseSrvResponse = HSE_ReadLifecycle(&HseAttrSecureLifecycle);
    LOGI("HseAttrSecureLifecycle: %d\r\n", HseAttrSecureLifecycle);

    /* read AttrExtendCustSecurityPolicy */
    HseSrvResponse = HSE_ReadAttrExtendCustSecurityPolicy(&HseAttrExtendCustSecurityPolicy);
    LOGI("HseAttrExtendCustSecurityPolicy: enableADKm = %d, startAsUser = %d\r\n", 
        HseAttrExtendCustSecurityPolicy.enableADKm, HseAttrExtendCustSecurityPolicy.startAsUser);

    /* copy active data to passive */
    HostFlash_PassiveUpgradeTest();
    LOGI("HostFlash_PassiveUpgrade success\r\n");

    /* ab swap */
    HseSrvResponse = HSE_ActivatePassiveBlock();
    if (HSE_SRV_RSP_OK != HseSrvResponse)
        LOGI("HSE_ActivatePassiveBlock fail [error_code: 0x%x]\r\n", HseSrvResponse);
    else 
        LOGI("HSE_ActivatePassiveBlock success\r\n");
}

#define MU0 (0)
#define HSE_ADMIN_CHANNEL (0)

hseSrvResponse_t HSE_ActivatePassiveBlock(void)
{
    hseSrvResponse_t hseStatus = HSE_SRV_RSP_GENERAL_ERROR;
    uint8_t u8MuChannel = HSE_ADMIN_CHANNEL; 
    hseSrvDescriptor_t* pHseSrvDesc;

    pHseSrvDesc = &gHseSrvDesc[MU0][u8MuChannel];
    memset(pHseSrvDesc, 0, sizeof(hseSrvDescriptor_t));

    pHseSrvDesc->srvId = HSE_SRV_ID_ACTIVATE_PASSIVE_BLOCK;
    hseStatus = HSE_Send(MU0, u8MuChannel, gSyncTxOption, pHseSrvDesc);

    /* wait for positive response */
    ASSERT(HSE_SRV_RSP_OK == hseStatus);
    return hseStatus;
}

 

screenshot-20230522-172325.png

0 件の賞賛
返信
6,192件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @liangyouchao 

please try to update the FW to latest version which is 0.2.6.0.

The correct file for AB Swap version (which ensures that OTA flag is enabled by HSE) is this one:

s32k3x2_hse_fw_1.13.0_2.6.0_pb221129.bin.pink

Update also the SBAF. It can be found in the 0.2.6.0 FW package too. It will ensure that all the HSE services will be available.

Regards,

Lukas

0 件の賞賛
返信
6,176件の閲覧回数
MengWang1
Contributor I

Hi Lukas,

I have updated HSE_FW_S32K3XX_0_2_6_0. How do I update SBAF

0 件の賞賛
返信
6,165件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

If you use scripts from the demo app, you can just select in T32:

lukaszadrapa_0-1685020521575.png

 The SBAF can be found here:

c:\NXP\HSE_FW_S32K3XX_0_2_6_0\hse_full_mem\sbaf\bin\s32k3x2_Secure_Baf_0.13.0_0.9.0_pb220502.bin.pink

 

Or it is described in the HSE Firmware Reference Manual in section 12.7 Secure-BAF update.

In short, it's necessary to load the pink file somewhere to flash and then call service HSE_SRV_ID_SBAF_UPDATE.

Regards,

Lukas

 

0 件の賞賛
返信
5,480件の閲覧回数
huangmingsong
Contributor III

Hi,I will update SBAF,but return HSE_SRV_RSP_NOT_ALLOWED,why ?

0 件の賞賛
返信