HSE – Install Firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HSE – Install Firmware

6,935件の閲覧回数
WXM
Contributor II

After S32K312_HSE_FW_INSTALL_V_0_1_2_1 is debugged, APP code cannot be burned?

WXM_1-1683254894457.png

WXM_2-1683254914908.png

 

After operation

WXM_3-1683255048693.png

 

 

 

0 件の賞賛
返信
6 返答(返信)

6,774件の閲覧回数
cg11
Contributor I

where can i get the “”S32K312_HSE_FW_INSTALL_V_0_1_2_1” Demo ?

0 件の賞賛
返信

6,770件の閲覧回数
WXM
Contributor II

找技术支持要的

0 件の賞賛
返信

6,759件の閲覧回数
cg11
Contributor I

可以分享一个吗?技术支持问了2次都没提供对。

0 件の賞賛
返信

6,911件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @WXM 

because part of the flash is reserved exclusively for HSE after FW installation, it is necessary to change the flash programming algorithm like on the attached screenshot. Then the Pemicro knows that it should not touch these areas and it will work as expected.

Regards,

Lukas

 

6,901件の閲覧回数
WXM
Contributor II
The version information is successfully obtained, indicating that the installation of HSE is successful???
0 件の賞賛
返信

6,906件の閲覧回数
WXM
Contributor II

Dear Lukas

The version information is successfully obtained, indicating that the installation of HSE is successful???

WXM_1-1683270518952.png

 

WXM_0-1683270458766.png

 

0 件の賞賛
返信