HSE – Install Firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HSE – Install Firmware

6,893 次查看
WXM
Contributor II

After S32K312_HSE_FW_INSTALL_V_0_1_2_1 is debugged, APP code cannot be burned?

WXM_1-1683254894457.png

WXM_2-1683254914908.png

 

After operation

WXM_3-1683255048693.png

 

 

 

0 项奖励
回复
6 回复数

6,732 次查看
cg11
Contributor I

where can i get the “”S32K312_HSE_FW_INSTALL_V_0_1_2_1” Demo ?

0 项奖励
回复

6,728 次查看
WXM
Contributor II

找技术支持要的

0 项奖励
回复

6,717 次查看
cg11
Contributor I

可以分享一个吗?技术支持问了2次都没提供对。

0 项奖励
回复

6,869 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @WXM 

because part of the flash is reserved exclusively for HSE after FW installation, it is necessary to change the flash programming algorithm like on the attached screenshot. Then the Pemicro knows that it should not touch these areas and it will work as expected.

Regards,

Lukas

 

6,859 次查看
WXM
Contributor II
The version information is successfully obtained, indicating that the installation of HSE is successful???
0 项奖励
回复

6,864 次查看
WXM
Contributor II

Dear Lukas

The version information is successfully obtained, indicating that the installation of HSE is successful???

WXM_1-1683270518952.png

 

WXM_0-1683270458766.png

 

0 项奖励
回复