HSE – Install Firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HSE – Install Firmware

6,937 Views
WXM
Contributor II

After S32K312_HSE_FW_INSTALL_V_0_1_2_1 is debugged, APP code cannot be burned?

WXM_1-1683254894457.png

WXM_2-1683254914908.png

 

After operation

WXM_3-1683255048693.png

 

 

 

0 Kudos
Reply
6 Replies

6,776 Views
cg11
Contributor I

where can i get the “”S32K312_HSE_FW_INSTALL_V_0_1_2_1” Demo ?

0 Kudos
Reply

6,772 Views
WXM
Contributor II

找技术支持要的

0 Kudos
Reply

6,761 Views
cg11
Contributor I

可以分享一个吗?技术支持问了2次都没提供对。

0 Kudos
Reply

6,913 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @WXM 

because part of the flash is reserved exclusively for HSE after FW installation, it is necessary to change the flash programming algorithm like on the attached screenshot. Then the Pemicro knows that it should not touch these areas and it will work as expected.

Regards,

Lukas

 

6,903 Views
WXM
Contributor II
The version information is successfully obtained, indicating that the installation of HSE is successful???
0 Kudos
Reply

6,908 Views
WXM
Contributor II

Dear Lukas

The version information is successfully obtained, indicating that the installation of HSE is successful???

WXM_1-1683270518952.png

 

WXM_0-1683270458766.png

 

0 Kudos
Reply