HSE IVT Auth_TAG

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HSE IVT Auth_TAG

1,951 次查看
liyongfeng
Contributor III

I used an offline tool to calculate the IVT GMAC, but the result differs from HSE's. I want to know how to obtain the same result based on applicationDebugKeyPassword[16U] = { 0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0a, 0x0b, 0x0c, 0x0d, 0x0e, 0x0f }?

liyongfeng_0-1747206681217.png

 

0 项奖励
回复
4 回复数

1,930 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Please provide further details about used example codes and mentioned tool. Thanks

0 项奖励
回复

1,889 次查看
liyongfeng
Contributor III

applicationDebugKeyPassword=000102...0F;

How to calculate the red part below using an offline tool to obtain the blue part's GMAC?

A5 5A A5 5A 09 00 00 00 00 00 00 00 00 60 44 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
C0 40 40 00 00 00 00 00 00 00 00 00 00 00 00 00
FF FF FF FF 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 79 AB 16 44 70 B3 B6 3D 4E 35 70 C1
44 E3 5F FC 7B 5A 1A E4 55 B3 03 C8 87 FA 25 A4

if __name__ == '__main__':
key = b'000102030405060708090A0B0C0D0E0F'
iv = b'79AB164470B3B63D4E3570C1'
data = b'A55AA55A090000000000000000604400\
00000000000000000000000000000000\
00000000000000000000000000000000\
C0404000000000000000000000000000\
FFFFFFFF000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
0000000079AB164470B3B63D4E3570C1'
aesgcm = AESGCM(key)
gmac = aesgcm.encrypt(iv, data, None)[-16:] # Last 16 bytes are GMAC
print(gmac.hex())

output:d6a5196d7573dd9bd49e9fce08ebb73b
It is different from the 16-byte IVT.GMAC shown in the figure above.
 

 

0 项奖励
回复

1,802 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Potentially the issue could be that you are using ASCII characters in Python script but HSE uses direct bin values i.e. HEX numbers

0 项奖励
回复

1,814 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

COuld you clarify which HSE example code you are referring to? Or describe how you do it on MCU side?

0 项奖励
回复