HSE IVT Auth_TAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HSE IVT Auth_TAG

1,885 Views
liyongfeng
Contributor III

I used an offline tool to calculate the IVT GMAC, but the result differs from HSE's. I want to know how to obtain the same result based on applicationDebugKeyPassword[16U] = { 0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0a, 0x0b, 0x0c, 0x0d, 0x0e, 0x0f }?

liyongfeng_0-1747206681217.pngliyongfeng_0-1747206681217.png

 

0 Kudos
Reply
4 Replies

1,864 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Please provide further details about used example codes and mentioned tool. Thanks

0 Kudos
Reply

1,823 Views
liyongfeng
Contributor III

applicationDebugKeyPassword=000102...0F;

How to calculate the red part below using an offline tool to obtain the blue part's GMAC?

A5 5A A5 5A 09 00 00 00 00 00 00 00 00 60 44 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
C0 40 40 00 00 00 00 00 00 00 00 00 00 00 00 00
FF FF FF FF 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 79 AB 16 44 70 B3 B6 3D 4E 35 70 C1
44 E3 5F FC 7B 5A 1A E4 55 B3 03 C8 87 FA 25 A4

if __name__ == '__main__':
key = b'000102030405060708090A0B0C0D0E0F'
iv = b'79AB164470B3B63D4E3570C1'
data = b'A55AA55A090000000000000000604400\
00000000000000000000000000000000\
00000000000000000000000000000000\
C0404000000000000000000000000000\
FFFFFFFF000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
00000000000000000000000000000000\
0000000079AB164470B3B63D4E3570C1'
aesgcm = AESGCM(key)
gmac = aesgcm.encrypt(iv, data, None)[-16:] # Last 16 bytes are GMAC
print(gmac.hex())

output:d6a5196d7573dd9bd49e9fce08ebb73b
It is different from the 16-byte IVT.GMAC shown in the figure above.
 

 

0 Kudos
Reply

1,736 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Potentially the issue could be that you are using ASCII characters in Python script but HSE uses direct bin values i.e. HEX numbers

0 Kudos
Reply

1,748 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

COuld you clarify which HSE example code you are referring to? Or describe how you do it on MCU side?

0 Kudos
Reply