Guidance for Basic PWM Configuration on NXP S32K312

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Guidance for Basic PWM Configuration on NXP S32K312

2,489件の閲覧回数
Mohmedsohel
Contributor III

Hello NXP Community,

I'm new to working with the S32K312 microcontroller and I'm trying to generate a basic PWM signal using the eMIOS module. I'm using S32 Design Studio and would appreciate any guidance or example code to get started with PWM generation.

My Setup:

  • MCU: S32K312
  • Tool: S32 Design Studio
  • PWM Module: eMIOS
  • Instance/Channel: Any basic example will do.

Questions:

  1. Can anyone share a simple code example with configuration or guide to configure and generate a PWM signal on the S32K312 using the eMIOS module?
  2. What are the key steps or important parameters to keep in mind while setting up PWM?
  3. Are there any existing tutorials or application notes that I can refer to for PWM configuration on this MCU?

 


 

タグ(4)
0 件の賞賛
返信
1 返信

2,475件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you have RTD installed then you can refer to basic PWM example called "Emios_Pwm_Ip_Example_S32K344" using low level driver or Pwm_example_S32K344 using MCAL level driver. If interesting in high level driver usage below thread can be very useful as well; https://community.nxp.com/t5/S32K-Knowledge-Base/RTD400-MCAL-K344-KEY-control-EMIOS-PWM/ta-p/1967347
And a recommendation is to read eMIOS chapter of the device RM for implementation info, available modes functionality etc. 

BR, Petr

0 件の賞賛
返信