Give Input from CAN to NXP Blocks

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Give Input from CAN to NXP Blocks

2,429 次查看
Akshay_idiada
Contributor II

We want to take inputs from CAN messages that is received and give these inputs to NXP blocks such as adc . pwm functions for S32k3xx.

Request your support as early as possible

标记 (1)
0 项奖励
回复
6 回复数

2,400 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this seems to be rather application question, so it is up to user how process/use received data from CAN module. 
I can just recommend to refer to available RTD demo examples for CAN/ADC/PWM or refer to more examples given at https://community.nxp.com/t5/forums/recentpostspage/interaction-style/tkb/post-type/thread/board-id/...

BR, Petr

0 项奖励
回复

2,393 次查看
Akshay_idiada
Contributor II

Yeah that is at application side but the query is that do we have any means to provide this CAN inputs to the NXP function Blocks because these blocks read inputs from the pin directly there is no option to provide external input to these blocks.

标记 (1)
0 项奖励
回复

2,381 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you are asking about signal multiplexing on MCU pad then refer to chapter 4 of the device RM and device IOMUX file attached to this document, to know which peripheral function can be assigned to each MCU pad

BR, Petr

0 项奖励
回复

2,284 次查看
Akshay_idiada
Contributor II
Hi,
The examples that you are referring contains only .c files. Can you share the reference for examples that contains the Matlab models?
0 项奖励
回复

2,237 次查看
Akshay_idiada
Contributor II
Hi ,
Can you share the examples that contains Matlab model ?
0 项奖励
回复

2,205 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

check MBDT community space for more info;
https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt

BR, Petr

0 项奖励
回复