Give Input from CAN to NXP Blocks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Give Input from CAN to NXP Blocks

2,381件の閲覧回数
Akshay_idiada
Contributor II

We want to take inputs from CAN messages that is received and give these inputs to NXP blocks such as adc . pwm functions for S32k3xx.

Request your support as early as possible

タグ(1)
0 件の賞賛
返信
6 返答(返信)

2,352件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this seems to be rather application question, so it is up to user how process/use received data from CAN module. 
I can just recommend to refer to available RTD demo examples for CAN/ADC/PWM or refer to more examples given at https://community.nxp.com/t5/forums/recentpostspage/interaction-style/tkb/post-type/thread/board-id/...

BR, Petr

0 件の賞賛
返信

2,345件の閲覧回数
Akshay_idiada
Contributor II

Yeah that is at application side but the query is that do we have any means to provide this CAN inputs to the NXP function Blocks because these blocks read inputs from the pin directly there is no option to provide external input to these blocks.

タグ(1)
0 件の賞賛
返信

2,333件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you are asking about signal multiplexing on MCU pad then refer to chapter 4 of the device RM and device IOMUX file attached to this document, to know which peripheral function can be assigned to each MCU pad

BR, Petr

0 件の賞賛
返信

2,236件の閲覧回数
Akshay_idiada
Contributor II
Hi,
The examples that you are referring contains only .c files. Can you share the reference for examples that contains the Matlab models?
0 件の賞賛
返信

2,189件の閲覧回数
Akshay_idiada
Contributor II
Hi ,
Can you share the examples that contains Matlab model ?
0 件の賞賛
返信

2,157件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

check MBDT community space for more info;
https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt

BR, Petr

0 件の賞賛
返信