Give Input from CAN to NXP Blocks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Give Input from CAN to NXP Blocks

2,432 Views
Akshay_idiada
Contributor II

We want to take inputs from CAN messages that is received and give these inputs to NXP blocks such as adc . pwm functions for S32k3xx.

Request your support as early as possible

Tags (1)
0 Kudos
Reply
6 Replies

2,403 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this seems to be rather application question, so it is up to user how process/use received data from CAN module. 
I can just recommend to refer to available RTD demo examples for CAN/ADC/PWM or refer to more examples given at https://community.nxp.com/t5/forums/recentpostspage/interaction-style/tkb/post-type/thread/board-id/...

BR, Petr

0 Kudos
Reply

2,396 Views
Akshay_idiada
Contributor II

Yeah that is at application side but the query is that do we have any means to provide this CAN inputs to the NXP function Blocks because these blocks read inputs from the pin directly there is no option to provide external input to these blocks.

Tags (1)
0 Kudos
Reply

2,384 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you are asking about signal multiplexing on MCU pad then refer to chapter 4 of the device RM and device IOMUX file attached to this document, to know which peripheral function can be assigned to each MCU pad

BR, Petr

0 Kudos
Reply

2,287 Views
Akshay_idiada
Contributor II
Hi,
The examples that you are referring contains only .c files. Can you share the reference for examples that contains the Matlab models?
0 Kudos
Reply

2,240 Views
Akshay_idiada
Contributor II
Hi ,
Can you share the examples that contains Matlab model ?
0 Kudos
Reply

2,208 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

check MBDT community space for more info;
https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt

BR, Petr

0 Kudos
Reply