Get specified temperature range for S32K116

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Get specified temperature range for S32K116

跳至解决方案
2,458 次查看
markus1
Contributor II

I'm using a S32K116 MCU with extended temperature range (-40...125°C) for my current project. I would like to detect if a wrong chip with the lower temperature range is assembled, because this could lead to expensive loss of function in the field.

Is there a register inside the chip that contains the temperature range information like the registers that contain information about the chip features (SIM->SDID)?

If not, is there some other way to detect the specified temperature range in software?

Thanks,

Markus

标签 (1)
0 项奖励
回复
1 解答
2,370 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I don't think it would be possible to detect it SW way. Such information is not stored in any MCU's register.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,371 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I don't think it would be possible to detect it SW way. Such information is not stored in any MCU's register.

0 项奖励
回复