How could use can interrupt to recieve can data with s32k144?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How could use can interrupt to recieve can data with s32k144?

1,814 Views
victor_song_171
Contributor III

Just like the title.

I want to use FlexCan Interrupt to recieve can data with the S32DS.How could I do? What config and code have to do ?

 

PS : Just use S32DS IDE and s32k144 SDK,not simulink and IAR.

0 Kudos
Reply
1 Reply

1,539 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

if you are using the SDK, the CAN driver installs and calls interrupts upon each transmit/receive operation, you need not to do any further setup. Just you can install a user callback function which will be called from MB interrupt and you can distinguish between several events.

See more info about interrupts here;Flexcan interrupt mode 

 

BR, Petr 

0 Kudos
Reply