FreeRTOS With S32K396

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRTOS With S32K396

3,772件の閲覧回数
jigs123
Contributor I

I am using FreeRTOS with S32K396 development package. I was getting OS option under S32DS to configure RTOS related parameters. 

 

jigs123_2-1680791364235.png

After recent update, OS Option is missing from above menu.

I have recently updated my S32K396 Development package with March 2023 release. I no longer get option to configure FreeRTOS under same menu. I do not see option to add FreeRTOS through SDK. Following are details of my S32K396 package version number. Can you please help me to get FreeRTOS configuration option under S32DS.

 

jigs123_0-1680791336290.png

jigs123_1-1680791350709.png

 

#S32K396

 

  

0 件の賞賛
返信
5 返答(返信)

3,737件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @jigs123 

If you have already installed the lasted FreeRTOS release for S32K3 platforms, you can add it on ConfigTools at Manage SDK Components (please refer to the below image).

VaneB_0-1681162953974.png

Whit this, you will be able to add FreeRTOS to your project.

 

B.R.

VaneB

0 件の賞賛
返信

3,733件の閲覧回数
jigs123
Contributor I

I have following version of RTOS installed.

jigs123_1-1681163886764.png

 

I do not see OS option in available SDK components.

 

jigs123_0-1681163857049.png

 

Can you please help me to understand what I may be missing.

 

0 件の賞賛
返信

3,727件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @jigs123 

Just to confirm, the package adds it to S32DS is SW32K3 FreeRTOS 10.5.0 version 3.0.0 CD2?

It seems that the package has not been installed correctly or does not support S32K396.

0 件の賞賛
返信

3,702件の閲覧回数
jigs123
Contributor I

When I try to install "SW32K3_FreeRTOS_10_5_0_CD2_3_0_0_DS_updatesite_D2301" package, I get message that "All Items are installed". So version is "SW32K3_FreeRTOS_10_5_0_CD2_3_0_0_DS_updatesite_D2301"

Is SW32K3_FreeRTOS_10_5_0_CD2_3_0_0_DS_updatesite_D2301 compatible with S32K396? If not which version should I use?

0 件の賞賛
返信

3,695件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @jigs123 

I made some test and the steps that I told you before just work with the S32K3 Real-Time Drivers Version 3.0.0 CD04 (SW32K3_RTD_4.4_R21-11_3.0.0_CD04_D2212_updatesite.zip).

Could you verify if this works for you?

0 件の賞賛
返信