FreeRTOS IIC_Deinit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS IIC_Deinit

3,025 Views
fancycang
Contributor I

Hi everyone

When I enable task scheduling and uninitialize the IIC module, an error occurs,becouse of OSIF_SemaDestroy(). why?

0 Kudos
Reply
5 Replies

3,024 Views
fancycang
Contributor I

I2C_MasterDeinit() and use flexio for iic

0 Kudos
Reply

2,985 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi

was I2C_MasterInit() called before, which should create osifSema?

BR, Petr

0 Kudos
Reply

2,979 Views
fancycang
Contributor I

Hi petr

I'm glad to receive your reply. I created a task and started task scheduling.

This is my code

I2C_MasterInit(&flexio_instance, &i2c_pal_flexio_MasterConfig0);
 
/* Initialize Interrupt priority for FlexIO I2C driver as bus master */
INT_SYS_SetPriority( FLEXIO_IRQn, configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY );
 
.........
 
I2C_MasterDeinit(&flexio_instance);
 
After this line of code  "(void)OSIF_SemaDestroy(&(master->idleSemaphore));"
 and the code jump to "portFORCE_INLINE static void vPortRaiseBASEPRI( void )"
I do not know how to receive this problem........
 
Best regards
0 Kudos
Reply

2,929 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

maybe this happens due to the lack of heap and stack of the task, so to avoid this try to increment the task's stack and the Total heap size.

BR, Petr

0 Kudos
Reply

2,924 Views
fancycang
Contributor I
Hi petr
i think my code heap and stack enough size
i finish this promble ,use function change i2c address
Best regards
0 Kudos
Reply