FlexCAN example communication

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FlexCAN example communication

1,723 次查看
935348277
Contributor I

I have an example project  of S42K144EVB FlexCAN,MCU is 100pin,when debuging,  CAN0  can't send message;i get the reason;   it's different in chip of CAN. S32K144EVB board   use   UJA1169TK/F,   But   the example project use MC33903,SO  !!!WHO  has the example project of  FlexCAN0,   By using  chip  of   UJA1169TK/F   thank you ! 

0 项奖励
回复
2 回复数

1,504 次查看
razva_tilimpea
NXP Employee
NXP Employee

Hi,

From where did you get this example? I think you are using an old SDK which works just for first silicon version. For 2 years or more that SBC is not supported in SDK because it was replaced by UJA1169.

Please try to get last SDK from S32DesignStudio and try to run the example project provided there.

Best regards,

Razvan

0 项奖励
回复

1,504 次查看
935348277
Contributor I

OK,I have solved  my problem, the UJA1169  should connect to 12V power source. 

0 项奖励
回复