FlexCAN configuration to enable switch from RUN to VLPR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexCAN configuration to enable switch from RUN to VLPR

1,558 Views
manujagrawal
Contributor II

Hi NXP team,

In RUN mode we have used PE clock as oscillator clock (8MHz) and module clock as SYS_CLOCK (80MHz). Since CAN can only support SIRC clock (8MHz) in VLPR, this may change the FLEXCAN bit rate (kbps) after switching from RUN to VLPR. Could you please suggest steps to manage the FLEXCAN driver and its configuration for smoothly switching from RUN to VLPR? 

Thanks and Regards 

Manuj Agrawal 

@danielmartynek 

0 Kudos
Reply
3 Replies

1,550 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

which driver do you mean? Assume SDK here...
If FlexCAN is using peripheral clock as PE clock still (CLKSCR=1) then it is enough to call FLEXCAN_DRV_SetBitrate() function to set new bitrates. it puts FlexCAN to freeze mode set bitrates and put module back to normal mode. There is an example to show this on https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K116-FlexCAN-VLPR-test-S32DS-ARM-2-2/ta-...

If PE clock must be changed then I think  FLEXCAN_DRV_Deinit() should be called and after mode switch init all again with new setting. CLKSCR can be changed when module is disabled. 

BR, Petr

0 Kudos
Reply

1,544 Views
manujagrawal
Contributor II

Hi @PetrS 

Thank you for your proposed solution. I think I can work with making the Peripheral Clock and PE Clock for an easy switch between RUN to VLPR. 

Could you also please help me understand importance of PE and Module Clocks in FLEXCAN and which different functionalities in the FLEXCAN are governed by them separately? 

Thanks and Regards

Manuj Agrawal

0 Kudos
Reply

1,534 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

refer to Table 27-9. Peripheral module clocking and chapter 55.5.10 Clock domains and restrictions of the reference manual.

BR, Petr

0 Kudos
Reply