FlexCAN Rx Mailbox Config to allow all CAN ID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexCAN Rx Mailbox Config to allow all CAN ID

ソリューションへジャンプ
5,931件の閲覧回数
soumyajit_das
Contributor I

MCU: S32K144

Hi,

I have imported the example project "S32K144_Project_FlexCan" in the S32 IDE. I see that the example shows how to accept data from a particular CAN ID (incoming messages). I would like to know how do we configure the registers to accept messages from any CAN ID (incoming).

I see there are three relevant register settings in FlexCAN:

1. RXMGMASK (Rx Mailboxes Global Mask register)

2. RXIMRx (Rx Individual Mask registers)

3. CAN  ID field of the MB Message Box Structure

In the given example, the registers RXMGMASK is set to 0xFFFF indicating that all bits of the incoming CAN Message ID needs to be considered. Same for RXIMRx also. In this case, when you configure MB CAN ID as (say) 555, then incoming messages with CAN ID 555 will only be allowed to be received by the Rx MB.

What if I want the Rx MB to receive any CAN message bearing any CAN ID? Is the required setting 'RXMGMASK=0x0000' & 'RXIMRx=0x0000'?

If yes, then what should we put in the Rx MB CAN ID field?

NOTE:

  1. I am using standard CAN ID only

  2. CAN FD (Flexible Data Rate) not used

  3. I am using FlexCAN0 of the MCU

Thanks

Regards

Soumyajit

Bosch, Bangalore

1 解決策
5,864件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport
2 返答(返信)
5,555件の閲覧回数
Andre_b
Contributor II

Hi

I read the solution proposed by Daniel but I didn't understand how to modify the example project "S32K144_Project_FlexCan" to obtain reading all message incoming with all available IDs.

In the example any message has the own ID buffer, so it can be read as below

RxID = (CAN0->RAMn[ 4*MSG_BUF_SIZE + 1] & CAN_WMBn_ID_ID_MASK) >> CAN_WMBn_ID_ID_SHIFT; /* Read ID

but without a buffer for reading ID and message, how can I read ID and datafield?

Thanks

Regards 

Andrea

0 件の賞賛
返信
5,865件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi [email protected],

It was answered here:

S32K148 CAN receiver without filtering 

Regards,

Daniel