Flashing using J-link in S32K148EVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flashing using J-link in S32K148EVB

734 次查看
Prajwal123
Contributor II

I am working on a S32K148EVB board. I want to flash the board using J-Link. What are the jumper connections I need to configure in the board so that the device is detected in the J-Link. Currently it shows low voltage. It seems the pin 1 of the JTAG (J5) is not getting the power supply. Is it due to jumper misconfiguration? If yes kindly help with the configuration and other things which might be affecting this

标记 (1)
0 项奖励
回复
2 回复数

686 次查看
IsaulO
NXP Employee
NXP Employee

Hi @Prajwal123

There is no specific jumper configuration for the board to use J-Link, whit the default configuration you should be able to do so.
You can see the default jumper configuration in Getting Started with the S32K148-Q176 Evaluation Board.
Also, if the problem occurs when J-Link is checking the target voltage please check if target is powered and if ribbon cable is plugged properly.

Untitled picture.png

BR,
IsaulO.

0 项奖励
回复

731 次查看
Prajwal123
Contributor II

Using J-Link segger pro

0 项奖励
回复