Flashing using J-link in S32K148EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing using J-link in S32K148EVB

719 Views
Prajwal123
Contributor II

I am working on a S32K148EVB board. I want to flash the board using J-Link. What are the jumper connections I need to configure in the board so that the device is detected in the J-Link. Currently it shows low voltage. It seems the pin 1 of the JTAG (J5) is not getting the power supply. Is it due to jumper misconfiguration? If yes kindly help with the configuration and other things which might be affecting this

Tags (1)
0 Kudos
Reply
2 Replies

671 Views
IsaulO
NXP Employee
NXP Employee

Hi @Prajwal123

There is no specific jumper configuration for the board to use J-Link, whit the default configuration you should be able to do so.
You can see the default jumper configuration in Getting Started with the S32K148-Q176 Evaluation Board.
Also, if the problem occurs when J-Link is checking the target voltage please check if target is powered and if ribbon cable is plugged properly.

Untitled picture.png

BR,
IsaulO.

0 Kudos
Reply

716 Views
Prajwal123
Contributor II

Using J-Link segger pro

0 Kudos
Reply