Flashing Custom S32k144 board using Open SDA Interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flashing Custom S32k144 board using Open SDA Interface

646 次查看
Jeevansagar
Contributor III

I am using the S32K144 evaluation board and would like to flash my custom board using the onboard debugger. I plan to use only the J106 (SWD DIO) and J8 (SWD CLK) pins for this purpose. However, I’ve seen community posts suggesting the use of the J14 10-pin header for flashing. Can I avoid using the J14 header and proceed with just the two pins? Is this approach possible?

标记 (1)
0 项奖励
回复
1 回复

624 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please see PEMicro's explanation for this:  Program/Debug issue with S32K142-Q48: Our OpenSDA interfaces are designed for evaluation purposes to debug and program the onboard target devices. They are not meant to be used to debug devices on external custom boards.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复