FS32K118 code Flash Erasable times

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS32K118 code Flash Erasable times

1,862件の閲覧回数
sunxiaoyi
Contributor I

问题:

      压力升级测试6W次,开始偶现FLASH擦除失败问题。 复现概率1/300

      擦除使用库函数 address = const 0x0000e000U,size = const 0x32000U:

     出现问题ret不为seccess。

    现在急需想寻求帮,flash可编程最大次数为? S32K-RM.pdf中是否有相关说明,如果有请指出。

谢谢。

uint16_t FlashErase(uint32_t address, uint32_t size)
{
	uint16_t ret = STATUS_SUCCESS;

	/*关全局中断*/
	INT_SYS_DisableIRQGlobal();

	/*erase*/
	ret = FLASH_DRV_EraseSector(&g_tflashSSDConfig, address, size);
	if(STATUS_SUCCESS != ret)
	{
		INT_SYS_EnableIRQGlobal();
		return ret;
	}
//	DEV_ASSERT(STATUS_SUCCESS == ret);

    /* Verify  */
    ret = FLASH_DRV_VerifySection(&g_tflashSSDConfig, address, size / FTFx_DPHRASE_SIZE, 1u);

    /*开全局中断*/
	INT_SYS_EnableIRQGlobal();

    return ret;
}

 

Question:

The pressure upgrade test was conducted for 6W times, and the flash erase failure problem began to occur occasionally. Recurrence probability 1/300

Erase using library function address=const 0x0000e000U, size=const 0x32000U:

 

When there is a problem, ret is not second.

 

Now we need help urgently. What is the maximum number of times flash can be programmed? Whether there are relevant instructions in S32K-RM.pdf. If yes, please indicate.

 

thank you.

 

 

0 件の賞賛
返信
1 返信

1,848件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @sunxiaoyi,

How many times did you erase the sectors?

Cycling endurance is guaranteed up to 1k cycles.

danielmartynek_0-1678958489493.png

 

Regards,

Daniel

0 件の賞賛
返信