FS26 driver Autocore compatibility issue?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS26 driver Autocore compatibility issue?

1,756件の閲覧回数
Oliver91
Contributor II

Hi,

I am trying to integrate the FS26 SBC device driver into a project with Autocore. The problem is that que Wdg_43_fs26 module is not loaded by the tresos so it is not available to be added to the project. 

I have tried both, the normal installation with the plugins linked to the tresos installation and the manual copy of both the  Sbc_fs26_TS_T40D34M40I0R0 and Wdg_43_fs26_TS_T40D34M40I0R0 folders into the Tresos plugins folder, but the result is the same in both cases.

The thing is that the Sbc_fs26 module is correctly loaded into the tresos module list, but the Wdg_43_fs26 does not appear in the module list no matter what.

Is there any kind of compatibility issue between the Autocore and this Wdg driver?

I have attached an image related with the issue. The MCU is the S32K344. The module and SW versions are the following ones:

EB Tresos 29.3.0

Autocore OS 6.1

SBC Driver: S32K3xx_SBC_FS26_R21-11_4.0.0

RTD Driver: SW32K3_S32M27x_RTD_R21-11_4.0.0_P19

Any help will be appreciated, thanks in advance.

 

タグ(4)
0 件の賞賛
返信
3 返答(返信)

1,498件の閲覧回数
Oliver91
Contributor II

Shall I assume this is a bug?

0 件の賞賛
返信

1,713件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi @quangvuanh,

Could you please help with this issue regarding the FS26 driver?

Thanks & BRs, Tomas 

0 件の賞賛
返信

1,748件の閲覧回数
Oliver91
Contributor II
Sorry, the RTD driver is the SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311, which I think is included with this Autocore release (Autocore 8.8.9 in the NXP download page)
0 件の賞賛
返信