FS26 SBC VDDIO pin current

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FS26 SBC VDDIO pin current

2,105 次查看
mogilipuri_harish
Contributor II

hello team

 

we are using FS26 in our deigns we need what is load current on VDDIO pin in FS26 SBC. 

0 项奖励
回复
5 回复数

2,086 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Harish,

unfortunately we do not have this value. There is many variables influencing the VDDIO current consumption. However, the VDDIO pin is recommended to be supplied from any of the FS26 regulators. Lowest power capabilities have LDO1 and LDO2. 400mA. So you can be sure, that the VDDIO power consumption is never higher, than 400mA. 

JozefKozon_0-1680586386410.png

JozefKozon_1-1680586433098.png

JozefKozon_2-1680586516290.png

With Best Regards,

Jozef

 

0 项奖励
回复

2,082 次查看
mogilipuri_harish
Contributor II

Hello

 

we are planning to connect this VDDIO pin from external LDO is it ok?

0 项奖励
回复

2,079 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Harish,

we are planning to connect this VDDIO pin from external LDO is it ok?

[A] Yes, you can use external LDO to supply the VDDIO.

With Best Regards,

Jozef

0 项奖励
回复

1,981 次查看
mogilipuri_harish
Contributor II

hello team

 

in OTP mode we need VDDIO supply before regulator power on. how is it possible if we connected VDDIO to SBC LDO's regulator output? refer figure 72 in product datasheet (DS616030-FS26 Product Datasheet 3.0(3.0)).

0 项奖励
回复

1,971 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Harish,

the VDDIO pin in the Figure 72. flowchart is meant as external event. Meaning that is valid, when the VDDIO pin is supplied from an external source.

JozefKozon_0-1681361410162.png

With Best Regards,

Jozef

0 项奖励
回复