FS26 SBC VDDIO pin current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS26 SBC VDDIO pin current

3,079件の閲覧回数
mogilipuri_harish
Contributor II

hello team

 

we are using FS26 in our deigns we need what is load current on VDDIO pin in FS26 SBC. 

0 件の賞賛
返信
5 返答(返信)

3,060件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Harish,

unfortunately we do not have this value. There is many variables influencing the VDDIO current consumption. However, the VDDIO pin is recommended to be supplied from any of the FS26 regulators. Lowest power capabilities have LDO1 and LDO2. 400mA. So you can be sure, that the VDDIO power consumption is never higher, than 400mA. 

JozefKozon_0-1680586386410.png

JozefKozon_1-1680586433098.png

JozefKozon_2-1680586516290.png

With Best Regards,

Jozef

 

0 件の賞賛
返信

3,056件の閲覧回数
mogilipuri_harish
Contributor II

Hello

 

we are planning to connect this VDDIO pin from external LDO is it ok?

0 件の賞賛
返信

3,053件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Harish,

we are planning to connect this VDDIO pin from external LDO is it ok?

[A] Yes, you can use external LDO to supply the VDDIO.

With Best Regards,

Jozef

0 件の賞賛
返信

2,955件の閲覧回数
mogilipuri_harish
Contributor II

hello team

 

in OTP mode we need VDDIO supply before regulator power on. how is it possible if we connected VDDIO to SBC LDO's regulator output? refer figure 72 in product datasheet (DS616030-FS26 Product Datasheet 3.0(3.0)).

0 件の賞賛
返信

2,945件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Harish,

the VDDIO pin in the Figure 72. flowchart is meant as external event. Meaning that is valid, when the VDDIO pin is supplied from an external source.

JozefKozon_0-1681361410162.png

With Best Regards,

Jozef

0 件の賞賛
返信