FLEXIO_UART_S32K144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FLEXIO_UART_S32K144

1,613件の閲覧回数
gongchangyu
Contributor I

image.pngIn the project of FLEXIO_UART_S32K144, , please help to assess whether there is a risk of FLEXIO_UART_DRV_CheckStatusTx. If the function of FLEXIO_UART_DRV_CheckStatusTx is set with a high bort rate of serial port, communication will fail if this code is not shielded.Can I block it?

0 件の賞賛
返信
1 返信

1,601件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello gongchangyu

This part of the code is to ensure that the timer gets an interruption when the transmission is complete. If you comment this part, the interruption won't be enabled.

 

If you have more questions do not hesitate to ask me.

Best regards,

Omar

0 件の賞賛
返信