FLEXIO_UART_S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FLEXIO_UART_S32K144

614 Views
gongchangyu
Contributor I

image.pngIn the project of FLEXIO_UART_S32K144, , please help to assess whether there is a risk of FLEXIO_UART_DRV_CheckStatusTx. If the function of FLEXIO_UART_DRV_CheckStatusTx is set with a high bort rate of serial port, communication will fail if this code is not shielded.Can I block it?

0 Kudos
1 Reply

602 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello gongchangyu

This part of the code is to ensure that the timer gets an interruption when the transmission is complete. If you comment this part, the interruption won't be enabled.

 

If you have more questions do not hesitate to ask me.

Best regards,

Omar

0 Kudos