FLEXIO_UART_S32K144

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FLEXIO_UART_S32K144

1,583 次查看
gongchangyu
Contributor I

image.pngimage.pngIn the project of FLEXIO_UART_S32K144, , please help to assess whether there is a risk of FLEXIO_UART_DRV_CheckStatusTx. If the function of FLEXIO_UART_DRV_CheckStatusTx is set with a high bort rate of serial port, communication will fail if this code is not shielded.Can I block it?

0 项奖励
回复
1 回复

1,571 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello gongchangyu

This part of the code is to ensure that the timer gets an interruption when the transmission is complete. If you comment this part, the interruption won't be enabled.

 

If you have more questions do not hesitate to ask me.

Best regards,

Omar

0 项奖励
回复