External rising edge triggers ADC sampling

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

External rising edge triggers ADC sampling

跳至解决方案
1,045 次查看
drfrefw123
Contributor I

I am using the chip s32k344 and want to use the external rising edge to trigger ADC sampling by configuring trgmux and adc.

drfrefw123_0-1706252645387.pngdrfrefw123_1-1706252668469.png

ADC port and trgmux port

drfrefw123_3-1706253510644.pngdrfrefw123_4-1706253523961.pngdrfrefw123_5-1706253537848.pngdrfrefw123_6-1706253593394.pngdrfrefw123_7-1706253611763.png

The external pwm is injected into the I/O port,But the program can't get in Notification

0 项奖励
回复
1 解答
1,001 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

eMIOS input cannot be selected as TRGMUX source, just eMIOS output.
Try to configure PTC11 for TRGMUX_IN10 functionality and config TRGMUX to select this TRGMUX_IN10 as input source for ADC external trigger.

BR, Petr

 

 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,002 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

eMIOS input cannot be selected as TRGMUX source, just eMIOS output.
Try to configure PTC11 for TRGMUX_IN10 functionality and config TRGMUX to select this TRGMUX_IN10 as input source for ADC external trigger.

BR, Petr

 

 

 

0 项奖励
回复